What is a Direct Acting Solenoid Valve?
Direct acting solenoid valves, also known as zero rated solenoid valves, are electro-mechanical valves that are used to control the flow of liquids or gases. This type of valve is directly actuated by the solenoid and does not require any difference in pressure between the inlet and outlet ports in order to operate; they can therefore function from 0 bar upwards.
27/04/2020

- You are here